Part Number: TMS320F280041
currently we are evaluating the TMS320F280041 for a new project and need information, if the analog comparator meet our requirements.
The project is a 4x interleaved PFC which has 4 times the below signal to switch off the PWMs. In total 8 comparator channels are needed to avoid reconfiguration during runtime.
The negative Input of the Comparators shall be set to 1.5V via the DAC's.
The PWM's are always running. Turn off shall be either due to timer (duty cycle) or if the comparator triggers.
Switching frequency is like 130kHz (full cycle e.g. between two red lines)
The transition pos->neg should switch off PWMxA
The transition neg->pos should switch off PWMxB
Is this possible without reconfiguration, if the comparators COMPH/COMPL are used?
How shall we connect the Analog signals to reach 8 PWMs, e.g. Pin9(CMP_HP0) & Pin12(CMP_LP1)?