Hi
I wish to communicate between two DSP 28335 boards. One in transmit mode and the other in receive mode.
I have two queries regarding this:
1. The transceiver I am using is VP233. Does it works fine on 3.3 V supply. Also do i need two separate transceivers?
2. I am not able to see any change in CANTA register and also CANES value is 0x00030010. What I understand from this is transmitter is not able to transmit.
What can be the probable reason for this error.
Thanks & Regards
Nitin