Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Dear sirs,
I am facing with the same error in loading firmware to flash memory.
I use IC REG LINEAR 1.2V 300MA for chip VDD.
I can successfully load "hello world" program to SRAM memory, but I can not load my specific program with InitSysCtrl() function.
I also can not load "hello world" program to FLASH memory.
Below is error report when I load my specific code to SRAM:
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.222.0)
C28xx_CPU1: Unable to determine target status after 20 attempts
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debuggin
Please give me some advices in this case.
Thank you so much!