Other Parts Discussed in Thread: C2000WARE, CONTROLSUITE
Hello,
trying to run example usb_dev_serial_m3 I have successfully imported, compiled and programmed F28M35x but Windws 8.1 (pro) device manager reports unknows device.
So reading information inside usb_dev_serial.c it says:
//***************************************************************************** //! \addtogroup master_example_list //! <h1>USB Serial Device (usb_dev_serial)</h1> //! //! This example application turns the evaluation kit into a virtual serial //! port when connected to the USB host system. The application supports the //! USB Communication Device Class, Abstract Control Model to redirect UART0 //! traffic to and from the USB host system. //! //! Assuming you installed MWare in the default directory, a //! driver information (INF) file for use with Windows XP, Windows Vista and //! Windows7 can be found in MWare/windows_drivers. For Windows //! 2000, the required INF file is in MWare/windows_drivers/win2K. //*****************************************************************************
I have pointed to driver location and tried to select all options provided (in picture it is Option1 and Option2) but it fails to recognize the device).
Should I download driver from another place or I am missing something?