Other Parts Discussed in Thread: TMS320F2812
Hi, all
In my recent project with CCS 3.3 and TMS320F2812, it is very strange that I can't set breakpoints in the CCS project program. My program was written in assembly language, when I flash the program into ROM and found that I can't set the hardware breakpoint in ROM. I did the following test to verify the problem:
1、In CCS2.2, I could set the hardware breakpoint in ROM, no matter whether the program was written in C or assembly language.
2、In CCS3.3, I could only set the hardware breakpoint in ROM when the program was written in C language.
So, my question is does the CCS3.3 support hardware breakpoint in ROM when the program is written in assembly language?