Part Number: LAUNCHXL-F28377S
Hi.
I try to make a Power Quality monitor with a DELFINO LAUNCHPAD F283777s or HERCULES LAUNCHPAD RML57Lx. PQ monitor should make a parallel sampling of 3 phase voltage with a rate to 1024 samples per cycle (0.061MSPS). I want to buy a ADS system to do sampling and then send digital data using a data interface like SPI,SCI, I2C. Is possible do the connection between DELFINO or RML57Lx and ADS system ?. If it's possible, have you any recommendation about ADS system, features, interface and others ?
Thank you for help
Best regards
David