Part Number: TMS320F28377S
Tool/software: Code Composer Studio
Hi everyone,
I established CAN communication using can_external_transmit code and ixxat usbtocan converter and I saw the messages on Minimon v3. And now, I want to establish CAN communication with DCAN_Boot.c example or flash_kernel_code examples. Is the transmiting and receiving message logic same ? In sci_flash_kernel code example, there are GetPacket and SendPacket functions. But in can flash kernel examples, GetPacket and SendPacket functions don't exist. Can I see the messages only using GetWordData and SendWordData functions ?
I have an another question. Do GetWordData function which is implemented in DCAN_Boot.c and CANMessageGet function which is implemented in can_external_transmit code example do same operation ?
Thanks and Regards.