Part Number: TMS320F28335
I am trying to synchronize the SVPWM pulses of two DC/AC converters using SYNCIN/SYNCO functionality of ePWM modules through CAN communication. But when external EPWMxSYNCI (hard-wire) connecting Sync_out pulse of master card to Sync_In of slave card, the ePWM signals are not synced & when using internal Software_Sync (SWFSYNC) bit to sync both PWM, there was continuous jittering of Slave card PWM observed with respect to master card PWM signals.
Request Mr.Prakash / anyone to guide me to sync PWM signals if this is achieved using SPI communication.