Part Number: TMS320F28069M
Other Parts Discussed in Thread: MOTORWARE, CONTROLSUITE
Hi all,
first at all I'm quite new to all this subject and read already a lot of manuals and helpful links, but still I'm confused.
I had the chance to receive a developer board with the TMS320 C2000 Piccolo chip on it. (github.com/.../TAPAS)
Now my plan was to put a motor on the board and controll it over an Arduino or ESP32 because i'm used to it. The development example just shows a Raspberry PI SPI control but I think I could convert that or adapt it in the equal programming language. But everytime when i search how to configure the drive correctly the speach is from InstaSpin or Motorware and if I understand it correctly therefor I need a JTAG adapter which i dont have.
Is there no solution to control the board over an arduino or configure it?
Also I have asked them if for example a recuperation is possible and the support (from the company the board is received) answered yes, but i have to take care of the maximum ratings. How do I set them?
I'm glad for every help :)
With regards,
Elektrolyt