This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28035: TMDSHVMTRINSPIN eQEP pin connection problem

Part Number: TMS320F28035
Other Parts Discussed in Thread: TMDSHVMTRINSPIN, TXB0106

Tool/software: TI C/C++ Compiler

TMDSHVMTRINSPIN eQEP pin connection problem:

1. What is the specific type of encoded output signal that the eQEP pin can receive? Is it affected by the chip TXB0106?

2. The output signals of most incremental photoelectric encoders are differential signals, which are A+, A-, B+, B-, I+, I-, respectively, but eQEP has only three pins. Are hardware connections only connected to A+, B+ and I+? How do we deal with the other three signal lines?

3. For this development board, does the RS-422 long-wire drive differential output or differential 5V output A+, B+, I+ match?

4.I signal level width has 1T, 1/2T and 1/4T difference, what difference in programming, and where to reflect?