Part Number: TMDSHVMTRPFCKIT
Other Parts Discussed in Thread: CONTROLSUITE
Hello, I am trying to connect the TMDSHVMTRPFCKIT to the EMJ-04APB22 motor for sensored control. I see that the motor has an encoder, but it is not clear where the signals should be connected to the test setup. I do however see the pinout of the encoder from the manufacturer's website. It is attached. I also see where TI specified to connect the encoder. It is also attached. The problem I am having is, the pins in the photo from TI are not labeled.
Also, is there a document that shows the names and locations of all of the pins that are on the TMDSHVMTRPFCKIT? I would like to see if has the ability allows the DSP to read any analog signals.
Thank you