This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28069ISO: Where can I find PCB of F2806x ISO controlCARD release 0.4

Part Number: TMDSCNCD28069ISO
Other Parts Discussed in Thread: C2000WARE,

1. Where can I find PCB of F2806x ISO controlCARD release 0.4?

2. Due to improper operation of the experiment, capacitor C25 and C202 have been damaged.Can these two capacitors be replaced or replaced by other capacitors?

3. When measuring the short circuit with multimeter, the test points TP1, TP2 and TP3 are all connected. Is U4 damaged?

  • user5220604,

    1. We do not sell blank PCBs of this design.
      1. The design files can be found in c2000Ware. 
      2. If you would like a new controlCARD you will need to purches the entire product TMDSCNCD28069ISO.
    2. If you damaged the capacitors you should replace them
      1. You should use an equal or more highly rated resistor.
    3. It is difficult to say.
      1. It is possible that other components have failed causing the short.

    Regards,
    Cody