Tool/software: TI C/C++ Compiler
Hi,
I know that simulator of F28335 is not officially supported but I am asking the question if someone had the same issue that I am facing but that found the solution.
I am using "simulator" of the F28335 to check first some processing without the need to be connected to a F28335 target.
I am also using the fast library: rts2800_fpu32_fast_supplement.lib.
Thanks to previous TI forum support, I am now able to run this fast library with the emulator (loading the ROM memory when using the simulator).
So now I was expecting to find exactly the same results on the target and with the simulator.
However now when I compare the results between Simulator and Real target I do not have the same results (some digit after the comma).
I checked the .map for two tests (Emulator, simulator) and it is the same. So I guess I have the same code.
Did you have already this issue?
Is it normal to have some differences in the processing results ?
Thanks for your support
Mathieu