Part Number: TMS320F28035
Other Parts Discussed in Thread: CONTROLSUITE, DRV8303, DRV8301
Since TMS320F28035 is used in DRV8303, I downloaded the CONTROLSUITE software, however I did not find any examples specific to DRV8303, so what are the examples and documentations compatible?
Also, does DRV8303EVM support standalone operation without instaspin GUI? Also, if I adjust the GUI to velocity control for example, Does the control loop take place in the microcontroller or the GUI? If it is on the microcontroller, can I set the DRV8303 to work on the velocity control using the GUI and then saving the parameters so that it can work on the velocity control but in standalone without the GUI? Thanks for help