Other Parts Discussed in Thread: SFRA, CONTROLSUITE
Hello,
We are trying to use SFRA library without GUI. We use CLA module to generate duty so we call SFRA_F_COLLECT and SFRA_F_INJECT within CLA isr (after execute CLA task). We execute SFRA_F_BACKGROUND every 1ms.
This is what we see in SFRA1 register:
start bit = 1
status is never bigger than 2
freqIndex = 0 (it is not increasing)
Is there any place where we can find the meaning of status bit? What reasons could cause freqIndex not increasing.
Best regards,
Paloma