This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: eCAP Capture Flag (CF) doesn't clear

Part Number: TMS320F28377S

I am using Matlab/Simulink 2017a with TIC2000 support package to develop software for a custom design. I am using an eCAP to capture the high and low time of a PWM signal so I can calculate the duty cycle.

It is reading the high and low counts properly. However when the signal is at 0% or 100% duty cycle the counts freeze (as expected) however the Capture Flag (CF) output stays at 1 even though I expect it to go to zero since there should be no capture happening.

Any thoughts?

Thanks,

Don