Other Parts Discussed in Thread: CCSTUDIO
I have had the High Voltage Motor Control and PFC Developer's Kit (TMDSHVMTRPFCKIT) fuses burn (250v 4~6.3 Amp) when AC power (110v) is plugged in to the kit. This happened after a failed real-time debugging session of HVPM_Sensorless_2833x_v15 (10/26/10) code with PMSM motor and F28335 control card on CCStudio 4.1 in FLASH mode. PFC was bypassed during the run. Is this common? Is there a work around for debugging?