Part Number: TMS320F28069M
Other Parts Discussed in Thread: UNIFLASH,
I used Uniflash to download boot code that tries to set the PLLCR registers etc. After the code is flashed I am not able to connect to it either with code composer or with uniflash. I get the following message when I try to run debugger in Code Composer:
Error connecting to the target:
(Error -1155 @ 0x0)
Device may be operating in low-power mode. The debugger has forced the device to wake up. Choose 'OK' to attempt to complete the debug connection.
(Emulation package 8.0.27.9)
If erasing all flash would fix the issue?
I am working with LaunchXL Launchpad for TMS320F28069M.