This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F2812 ADC Shift

Hi, Champs,

Customer is encountering with ADC issues when using F2812.

Some chips can sample the voltage range from about 20mV to 3V exactly but fail to sample the voltage under 20mV, whose ADC result will be same as the one when ADC input is 20mV.

While some chips can sample the voltage range from about 0V to 2.96V exactly but fail to sample the voltage above 2.96V, whose ADC result will be same as the one when ADC input is 2.96V.

It seems there is vacuum in the boundary (either the 0V or 3V), and we can't calibrate it with software way to compasate the like we do to the gain error and offset error.

So do you have any suggestions on it? Thanks for the information.

 

Best regards,

Ricky Zhang

  • Ricky,

    This is comprehended in the DS specs for this device's ADC as gain error and offset error.  These are +/-200(at FSR) and +/-80LSBs respectively, this overlaps the areas you and customer are seeing that are saturated early.  As you have noted on this device there is no way to recover these regions with SW calibration; this is essentially a keep out zone for the customer and their analog input.

    Best,

    Matthew

  • Matthew,

    Thanks for the confirmation, and I've told customer to keep this zone out. Thank you.

     

    Best regards,

    Ricky Zhang