This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What units is AdcMirror.ADCRESULT2 in

When I am watching the AdcMirror.ADCRESULT2 in the IDE watch window, what am I seeing?

I had been assuming that the A to D was showing milli-volts, but that does not match my other instruments.

Will

  • Hi William,

    The ADC Module converts the analogue voltage you apply to the ADC input into a 12 Bit digitized value. So what you see in the ADCRESULT Registers is a value between 0 and 4096 corresponding to a voltage between 0 and 3.3V respectively.

    Best regards

    Andreas

  • William Friesen said:

    When I am watching the AdcMirror.ADCRESULT2 in the IDE watch window, what am I seeing?

    I had been assuming that the A to D was showing milli-volts, but that does not match my other instruments.

    Will

    Andreas is correct.  One note though, you don't mention which device you are using.  If it is a 280x, 2833x, for example the ADC range is 0-3.0V.  While on 2803x and 2802x the analog input is 0-3.3V.  You mention the mirror registers so I believe it is one of the 0-3.0V devices.

    Please refer to the ADC manual for your particular device for more details.

    -Lori