This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMTRINSPIN: Is there recommended PN of MOTER(AC INDUCTION with ENCODER )?

Part Number: TMDSHVMTRINSPIN


Dears:

Is there recommended PN of MOTER(AC INDUCTION with ENCODER )?

Since there is no Moter in the KIT.

Pls. help to recommended PN or give your debugged PN.

  • I believe the Marathon (5K33GN2A) motor with encoder used to be available with the high voltage hit (HVKIT) before, but I can't find it on the TI site now. You can try searching TI.com for it yourself, or order elsewhere. In general, a 160~220VAC/50~60Hz/1kw ACI motor can be supported by the HVKIT

    Sean