For the selection of TMS320F28035PAGQ crystal, how can I check the performance of crystal (e.g. frequency tolerance, frequency stablility and aging) meet the requirement of MCU. Now, we are using 20MHz crystal (AA20000002 from TXC, specification is shown at below) and the system clock frequency of MCU is 60MHz.
We have a CAN flash failure at low temperature from -20~0oC. What advice would you have for this kind of problem?