Other Parts Discussed in Thread: MOTORWARE, CC2640
Tool/software: TI C/C++ Compiler
Hi,
I'm working on a project that i took over from a colleague,
When adding support for CC2000 devices with the ''CCS"->help/install new software C2000 device support, code composer does not give any errors (neither after the automatically restart).
Taking a look at the CCS->help/install new software, C2000 device support displays: All items are installed.
Next up, import a project (ti motorware):
Import CCS projects,
C:\ti\motorware\motorware_1_01_00_18\sw\solutions\instaspin_foc\boards\drv8301kit_revD\f28x\f2806xF
Import: proj_lab05b parses error:
See details below.
Error: Import failed for project 'proj_lab05b' because its compiler definition is not available. The project does not appear to be a CCS Project. Please try importing it using the 'General > Existing Projects into Workspace' wizard.
I took a look in my compiler installation directory: c:/ti/ccsv8/tools/compiler
This only shows me some arm compilers.
I've copied my colleagues compilers from his 'ccsv8/tools/compiler' directory to mine, however my workspace still does not detect it.
Is there any possible way, except from reinstalling all of CCS, to add the compiler manually?
Regards,
Daan