Part Number: TMDXHVMTRKIT5X
Other Parts Discussed in Thread: HVPMSMMTR
I bought a TMDXHVMTRKIT5X and HVPMSMMTR, follow doc(QSG-TMDSHVMTRKIT5X-GUIv1) step by step to make motor running,but there are some probems:
1/Motor's earth pin is floating, when i touch the motor ,I get an electric shock,but when i used a wire connect the pin to earth ,the motor dosn't work!!!!
2/The motor is serious heating! turn motor to 300rpm with unloading,after 1 min the temperature rice to more then 80 degrees Celsius!!!
Are these two conditions normal?