Part Number: LAUNCHXL-F28027F
Other Parts Discussed in Thread: MOTORWARE, CONTROLSUITE, BOOSTXL-DRV8301
Hi to All!
I want sinusoidal driving a sensored (hall sensors) BLDC motor, without PID loops, just speed control and direction, speed comant i want to be from PWM 20Khz 0%-100%.
I find a application AVR449 but use analog input for control.
I have one LAUNCHXL-F28027F and LAUNCHXL-F28027, i dont have the knowledge to do on C, i can do that with F28027? if yes can someone to drive me with some help to do?
or someone all ready do it with other MCU?
thanks