This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35H52C: Ethernet UDP communicaiton between M3 and Host PC

Part Number: F28M35H52C
Other Parts Discussed in Thread: CONTROLSUITE

Hi am trying to set up Ethernet UDP communication between M3 and host pc using Simulink with DHCP. The problem here is that I am able to send data from M3 to host but having trouble sending data from host to M3. 

I have attached the Simulink model and generated C codes, this is a very simple model just to test Ethernet function.

I also tried to use Static IP configuration but there were no connected established and I could not send data from M3 to host nor from host to M3. I did use jumpers on board mux 1-15, row b and c. 

Will be appreciated if someone can identify the problem here. 

Best regards,

Andrew  UDP.zip