This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

developement logic board for motor drive inverter



C2000™ 32-bit microcontrollers

I am looking for a development logic board for a development inverter ( 150KW, 20 000rpm , 400V DC) for our lab that would be able to

  • Sample signals for at least 2 current sensors
  • Measure one or more high voltages
  • Generate and read the signals of a resolver( or other position sensor)
  • Read and transmit CAN messages
  • Using  a Piccolo, Delfino or Hercules microcontroller

 I have found development kits for motor drive in the TI website but they have a low power inverter integrated on the same PCB. I would to know if  TI has something that would match my requirements.