I'm researching whether the C2000 microcontrollers (specifically the F28004x series) are a good fit for a project utilizing BLDC motors that I am currently working on. I had two quick questions after reviewing users guides, training videos, and forums.
- In the InstaSPIN User’s Guide, it states "FAST requires 2-phase currents (3 for 100% over-modulation)..." - is the 100% over-modulation just to utilize space-vector schemes?
- In order to utilize the FAST encoders, does the DC bus voltage of the motor have be monitored (i.e. sent to an on-board ADC) or is it optional?
Thanks.