Part Number: TMS320F2806
Hello,
We are having an issue with the high voltage Instaspin kit we are using to control our BLDC motor. We are using the original GUI for TMS320F28069 to spin the motor. The problem is that we are not able to get the maximum torque we need at start up. We tried both torque mode and "torque+speed" mode but the maximum starting torque we are getting is about 1.2 NM when we set the torque reference to 1 pu which is not able to spin our load. ( we have no problem at no load) The motor is designed to deliver higher starting torques. Currently, we are using the .out file provided by TI for TMS320F28069 GUI composer. Any suggestions how we could get higher torque? This is URGENT so we highly appreciate your quick response. Thanks!