This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F280049: SCI Example with ControlCard showing Garbled data

Part Number: TMS320F280049
Other Parts Discussed in Thread: C2000WARE

Tool/software: Code Composer Studio

Hi,

I'm trying to get the TMDXDOCK280049M working with the Code Composer C2000Ware SCI examples (sci_ex1_echoback, sci_ex2_interrupts, and sci_ex3_interrupts_fifo). I have connected the SCIARX and SCIATX on the board via pins 76 and 78 (based on TMDSCNCD28004x_RevA_120cCARD_pinout.pdf)  to my RS232 data connection, but I'm only seeing garbled data right now and no echoback. Perhaps, I'm missing something?

I have the S1-A switches both set to 'down' and the S1 left switch set to down. I'm using the JTAG on the ControlCard and powering the ControlCard via USB.

I've configured my serial connection in PuTTY as 9600 baud, 8 data bits, 1 stop bit, no parity, no hardware control.

Example sets of data returned on PuTTY during startup:

▒▒▒▒o5''!▒Q!▒▒▒▒M!▒-''▒5#5=▒9/=95▒=#7▒/5▒wY_▒-''▒59/!▒-▒;=9)▒▒▒▒▒o5''!▒Q!▒▒▒▒M!▒-''▒5#5=▒9/=95▒=#7▒/5▒wY_▒-''▒59/!▒-▒;=9)▒▒▒u#5=▒9/=95▒▒▒▒▒▒o5''!▒Q!▒▒▒▒M!▒-''▒5#5=▒9/=95▒=#7▒/5▒wY_▒-''▒59/!▒-▒;=9)▒▒k▒▒▒T▒Z▒▒▒▒▒M!▒5#▒▒▒▒▒▒u#5=▒9/=95▒▒

Thanks in advance for your help,

-Wes