Tool/software: Code Composer Studio
Hello, all:
I usually run the F28069 project under windows os environment on desktop.
And generate .hex and .bin with 'AppCode_COFF2BIN_F28069.bat' file.
The command in the batch file is as shown below:
------------------------------------------------------------------------------------------
" hex2000.exe AppCode_hex_F28069.cmd
FileIOShell.exe -i abc_F28069.hex -o abc_F28069.bin "
------------------------------------------------------------------------------------------
The command in AppCode_hex_F28069.cmd is as shown below:
------------------------------------------------------------------------------------------
"abc_F28069.out
-map abc_F28069_hex.map
-o abc_F28069.hex
-m
-memwidth 16
-image
ROMS
{
FLASH28069: origin = 0x3D8000, len = 0x1C000, romwidth = 16, fill = 0xFFFF
} "
------------------------------------------------------------------------------------------
For those required files (hex2000.exe / FileIOShell.exe / AppCode_hex_F28069.cmd / abc_F28069.out) are all located in Debug document inside project.
It works normally on CCS V6.1.3 (windows version) and can generate .hex and .bin successfully.
It also can work on CCS V6.2.0 (Mac version) originally.
But currently when I run the same project on the same MacBook and CCS environment, it can not generate .hex and .bin file.
Even after updating to CCS V8.2.0 (Mac version), it still doesn't work.
The error message is as shown below:
~/AppCode_COFF2BIN_F28069.bat" makefile:284: recipe for target 'post-build' failed ~/AppCode_COFF2BIN_F28069.bat: line 1: hex2000.exe: command not found ~/AppCode_COFF2BIN_F28069.bat: line 2: : command not found ~/AppCode_COFF2BIN_F28069.bat: line 3: FileIOShell.exe: command not found ~/AppCode_COFF2BIN_F28069.bat: line 4: : command not found ~/AppCode_COFF2BIN_F28069.bat: line 5: : command not found gmake[1]: [post-build] Error 127 (ignored)
This problem got my stumped for few days.
Would you please help me to solve it?
Thanks~!