Hi Ti Community!
I'm working with the TMS320f28335 and using the eQEP Module. I got a motor witch give me a special quadrature pulse signal.
It looks like the folowing scheme:
Count | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | 9 | 10 | 11 | 0 |
Channel A | 0 | 0 | 1 | 1 | 0 | 0 | 1 | 1 | 0 | 0 | 1 | 1 | 0 |
Channel B | 0 | 1 | 1 | 0 | 0 | 1 | 1 | 0 | 0 | 1 | 1 | 0 | 0 |
Index | 1 | 1 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 |
Its easy to see that the index signal is a complete Channel A period long, and the eQEP documentation permit a Index Signal like this (at the beginning of the Document --> Gated Index Signal). But I get a lot of problems when I implement it in the DSP.
The Counter Register of the QEP modul reset twice - first at the normal 0 Position and then at the Position 2.
TI Specialist, did you have a solution or Idea for that ?
Thanks a lot,
Heiko