Part Number: TMS320F28374S
Tool/software: Code Composer Studio
Hi,
I'm having a strange error when I try to connect a board with a 374S device.
Until now I've used the 377S and 379S without any problem.
Now I'm try to use the 374S device but when I start the debug procedure I receive the follow error:
I take a look into the F28374S.gel file and at row 82 I found the command:
The error cames when the debugger try to write 0x0FFF value to location 0x5F452, to initialize the GS0-GS11 memory blocks.
If I change the value to 0x00FF all works well.
If I set the value greater than 0xFF the error appears.
At this point I don't understand why the initialization of the GS8-GS11 blocks generate the debugger error.
Note that when I'm connect to the board and write manually the GS INIT register to 0x0FFF the initialization ends without error.
This is the DSP picture:
Can anybody give me an hint?
Thank you
Regards
Giuseppe