I would like to interface my Tamagwa Resolver, using this boosterxl-posmgr, with Launchpad F28379D. The problem is that my resolver needs an excitation voltage of 7 Vrms at 10Khz, in the user guide (of the boosterxl-posmgr) I read that it must be powered at 5V, but there is a table, shown in the figure, where it speaks of excitation voltage of 15 V. So I did not understand if I can implement this interface.