Part Number: TMS320F28379D
Hi,
For EMIF support CS0, the SDRAM supports different bank size but there is a confusion on the number that it supports.
In the register field description of SDRAM_CR Register, it says as follows
IBANK 000: 1 bank SDRAM devices.
001: 2 bank SDRAM devices.
010: 3 bank SDRAM devices.
011: 4 bank SDRAM devices.
1xx: Reserved.
But in the Table 25-8. Description of the SDRAM Configuration Register (SDRAM_CR) in the section 25.3.5.3 SDRAM Configuration Registers (spruhm8g.pdf), it says as follows
• When IBANK = 0h, 1 internal bank is used
• When IBANK = 1h, 2 internal banks are used
• When IBANK = 2h, 4 internal banks are used
Can you confirm what is the correct usage and the number of banks supported for SDRAM for EMIF_CS0?
Thanks,
Aditya