Part Number: TMS320F28069
Tool/software: Code Composer Studio
Hello,
I have started getting the following error.
Debug Initialization Error
Cannot read System Setup data from XML file C:\ti\CONTRO~1\DEVELO~1\OSKAR6~3\OSKAR6~1\XRECTI~1.CCX
Error parsing file "C:\ti\ccsv6\ccs_base\common\targetdb\drivers\TI_reg_ids\TMS470R53X_regids.xml":
Register id 0x8C00000000000000 is over 32 bits at line 69 column 71
I am not able to program the µC at all. Everything was working good yesterday. I guess it has something to do with the CCS update for TI Emulators. The first thing I did after opening the CCS is installing the update and after that the software is running into some kind of problems.
Could anyone please help?
Below is the screenshot of the error.