This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: C2prog program fail

Part Number: TMS320F28335


Tool/software: Code Composer Studio

Set GPIO 87/86/85/84 as 1110, set to SCI mode.

Set GPIO 37/34 as 01.

when use C2prog, it showed as below.

This SCI cable can work with F28062 normally.

Pls kindly suggest.

  • Hi,

    I hope you're using GPIO28 and 29 for bootloading.

    Regards,
    Gautam
  • Yes, GPIO28/29 is used for boatloading.

  • Hi - Can you please confirm that the frequency of your external crystal/oscillator is indeed 24 MHz?
    Also, please upgrade to the most recent 1.7 release of C2Prog. Version 1.5 is no longer supported.

    www.codeskin.com/c2prog-download
  • have tried version 1.7/1.6/1.5 , same error.

     external crystal/oscillator is 30.3M

    And revised the baud rate in config file from 3400-115200. But still no improve.

  • Piero,

    Did you try to contact Codeskin directly at info@codeskin.com on this issue?
    If not, please contact them. That will get you fast response.

    Thanks and regards,
    Vamsi
  • Piero,

    It is extremely important that you select a target configuration with matching clock frequency.

    Please take a moment to read the C2Prog manual, accessible from the help menu, which stresses this fact and provides other useful information.

    Since C2Prog currently does not provide a 30.3 MHz, I have generated a custom configuration for you. Please save it to the C2Prog "targets" folder.

    <?xml version="1.0" encoding="UTF-8"?>
    <targets>	
    	<configs>
    		<config>
    			<name>28235,335_30.3MHz</name>
    			<overrides>28235,335_30MHz</overrides>
    			<settings>
    				<primary>
    					<bootrecord>400;5760;1ce;9;51eb;1b4;1;0;0;0;0;0;0;0;0;0;f906</bootrecord>
    				</primary>	
    			</settings>
    		</config>		
    		<config>
    			<name>28235,335_30.3MHz-JTAG</name>
    			<overrides>28235,335_30MHz-JTAG</overrides>
    			<settings>
    				<primary>
    					<bootrecord>400;5760;1ce;9;51eb;1b4;1;0;0;0;0;0;0;0;0;0;f906</bootrecord>
    				</primary>	
    			</settings>
    		</config>
    	</configs>
    </targets>
    

  • Hi Codeskin,

    I'm sorry that my typo error for 30.3M, It should be 33.33M.

    Can you help to release another file for 33.33M?

    Thanks a lot.

  • Piero,

    Did you resolve this with CodeSkin offline? OR
    Are you still looking for help?

    Thanks and regards,
    Vamsi
  • Here is a 33.33 MHz configuration file.

    <?xml version="1.0" encoding="UTF-8"?>
    <targets>	
    	<configs>
    		<config>
    			<name>28235,335_33.33MHz</name>
    			<overrides>28235,335_30MHz</overrides>
    			<settings>
    				<primary>
    					<bootrecord>400;9350;1fc;8;9fbe;1aa;1;0;0;0;0;0;0;0;0;0;f34e</bootrecord>
    				</primary>	
    			</settings>
    		</config>		
    		<config>
    			<name>28235,335_33.33MHz-JTAG</name>
    			<overrides>28235,335_30MHz-JTAG</overrides>
    			<settings>
    				<primary>
    					<bootrecord>400;9350;1fc;8;9fbe;1aa;1;0;0;0;0;0;0;0;0;0;f34e</bootrecord>
    				</primary>	
    			</settings>
    		</config>
    	</configs>
    </targets>
    

  • Piero,

    Can I consider this thread closed? Or Do you need further related help?

    Thanks and regards,
    Vamsi
  • Piero,

    I am closing this post. Please open a new thread as needed.

    Thanks and regards,
    Vamsi