This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: Debugger Simulink Embedded Coder ?. SVM Generation

Part Number: TMS320F28069M

Dear TI-Team,

 I'm working on Code Generation in Simulink using Embedded Coder Package for C2000. In a simple example i want to generate a rotating SVM-Vector at low frequency and with that the motor should rotate with the same frequency of the SVM (as described in the attached picture). 

After the code was loaded on the processor, the motor (a Roxxy outrunner 6362) starts very hard and spins for short time. After 1 second all signals e.g. PWM, Gate-Signal are getting lost. 

So two questions about this issue:

+ do you have any suggestion to debug this issue and figure out what is the reason of losing all signals after the hard start?

+ I 'm assuming there are some issues with the over voltage  or too high current, what need to be changed to avoid the occurrence of those problem?. 

Many thanks in advance for your help.

Best regards,

Giang To