Part Number: TMS320F28020
Tool/software: Code Composer Studio
Hello,
is there a simple way using CCS to program multiple Piccolos in one JTAG chain with the exact same software? And how is it about multiple JTAG chains?
Regards,
Martin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28020
Tool/software: Code Composer Studio
Hello,
is there a simple way using CCS to program multiple Piccolos in one JTAG chain with the exact same software? And how is it about multiple JTAG chains?
Regards,
Martin
Martin,
There are options in CCS and some options outside of CCS:
1)Inside CCS:
a)The most basic way would be to manually select the processor in the chain and load the program directly
b)Through the use of either the scripting console or the DSS server you should be able to automate this so that it can be kicked off like a batch file to basically select the individual cores and load the code. There are scripting examples inside the ccsbase directory of the Code Composer install
2)Outside CCS:
Elprotronic make a tool that can program 8 devices in parallel through the JTAG interface. http://www.ti.com/tool/C2000-GANG This method does not need CCS IDE to be open/connected at all.
Best,
Matthew