Part Number: TMS320F28035
Team,
I’m working with a customer that is going to be using F28035 on their design. Originally they just used the F28035 ISO control board as is but they are in the process of consolidating multiple different cards into one and have some questions regarding the F28035 ISO EVM and schematic. The ISO boards that they have on hand appear to show some visible rework (wire jumpers) and they would like to know that these changes are actually reflected on the F28035 schematic.
Another question they had was about programming the device, if they are planning to use XDS100 programmer or gang programmer that already contains EEPROM and FT2223 (USB to UART) they would not need to copy those device from ISO control board to their own schematic once they consolidate these boards?
Thanks for looking into this!
Regards
Dmitry