This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: Help for switching frequency for sinusoidal PWM for three phase inverter

Part Number: TMS320F28335

Tool/software: Code Composer Studio

Hi,

I am trying to generate sinusoidal pwm for inverter and switching frequency should be between 4 kHz and 100 kHz but i cannot generate pwm above 70 kHz switching frequency. I think the problem is related with adc but i cannot solve it. Please help me.

My whole code is:
#include "DSP2833x_Device.h" #include <math.h> # define PI 3.14159265358979323846 /* pi */ ///////////////////////////////////////////////////////////////////////////////////////////////// // //////////////////////////////////////////////////////////////////////////////////////////// // // // long switchingFrequency=100000;// = 48000; // switching frequency in Hz // // // // float fundamentalSinusoidalFrequency = 50; // sinusoidal output frequency in Hz // // // // double phaseAngle = 0; // starting angle of sinus // // // // float fundamentalSinusoidalMagnitude = 3.3;//Peaktopeak Value of output sinus waveform // // long RisingEdgeDelay = 50; // Rising Edge Delay = TTBCLK x DBRED(=RisingEdgeDelay) long FallingEdgeDelay = 50; // Falling Edge Delay = TTBCLK x DBFED(=FallingEdgeDelay) // TTBCLK = 13.3333ns to give 666ns delay we can use that number /////////////////////////////////////////////////////////////////////////////////////////// // // //////////////////////////////////////////////////////////////////////////////////////////////// long deviceClockFrequency = 150000000; // f28335 clock frequency in hz float maximumDeviceVoltage = 3.3; // maximum voltage provided by device pin which 3.3V double counter = 0; double frequencyModulationRatio =0; float magnitudeModulationRatio = 0; float sinus=0; float sinus2=0; float sinus3=0; int CLKDIV = 1; int HSPCLKDIV = 1; float voltage_vr1; float voltage_vr2; float voltage_vr3; float voltage_vr4; // Prototype statements for functions found within this file. void Gpio_select(void); extern void InitSysCtrl(void); extern void InitPieCtrl(void); extern void InitPieVectTable(void); interrupt void ePWMA_compare_isr(void); interrupt void cpu_timer0_isr(void); void Setup_ePWM(void); extern void display_ADC(unsigned int); extern void InitAdc(void); interrupt void adc_isr(void); //########################################################################### // main code //########################################################################### void main(void) { InitSysCtrl(); // Basic Core Initialization EALLOW; SysCtrlRegs.WDCR = 0x00AF; EDIS; DINT; // Disable all interrupts Gpio_select(); // GPIO9,GPIO11,GPIO34 and GPIO49 as output (LEDs @ peripheral explorer) Setup_ePWM(); InitPieCtrl(); InitPieVectTable(); ////////////////////////////////////////////////////////////////////////////////////////// InitAdc(); AdcRegs.ADCTRL1.all = 0; AdcRegs.ADCTRL1.bit.SEQ_CASC = 1; // cascaded Sequencer Mode AdcRegs.ADCTRL1.bit.CONT_RUN = 0; // Single Run Mode AdcRegs.ADCTRL1.bit.ACQ_PS = 7; // 8 x ADC-Clock AdcRegs.ADCTRL1.bit.CPS = 0; // divide by 1 AdcRegs.ADCTRL2.all = 0; AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1 = 1; // ePWM_SOCA trigger AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1; // enable ADC int for seq1 AdcRegs.ADCTRL2.bit.INT_MOD_SEQ1 = 0; // interrupt after every EOS AdcRegs.ADCTRL3.bit.ADCCLKPS = 3; // set FCLK to 12.5 MHz AdcRegs.ADCMAXCONV.all = 0x0003; // 4 conversions AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0; // 1st channel ADCINA0 AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 1; // 2nd channel ADCINA1 AdcRegs.ADCCHSELSEQ1.bit.CONV02 = 2; AdcRegs.ADCCHSELSEQ1.bit.CONV03 = 3; EPwm5Regs.TBCTL.all = 0xC030; // Configure timer control register /* bit 15-14 11: FREE/SOFT, 11 = ignore emulation suspend bit 13 0: PHSDIR, 0 = count down after sync event bit 12-10 000: CLKDIV, 000 => TBCLK = HSPCLK/1 bit 9-7 000: HSPCLKDIV, 000 => HSPCLK = SYSCLKOUT/1 bit 6 0: SWFSYNC, 0 = no software sync produced bit 5-4 11: SYNCOSEL, 11 = sync-out disabled bit 3 0: PRDLD, 0 = reload PRD on counter=0 bit 2 0: PHSEN, 0 = phase control disabled bit 1-0 00: CTRMODE, 00 = count up mode */ EPwm5Regs.TBPRD = 10999; // TPPRD +1 = TPWM / (HSPCLKDIV * CLKDIV * TSYSCLK) // = 20 µs / 6.667 ns EPwm5Regs.ETPS.all = 0x0100; // Configure ADC start by ePWM2 /* bit 15-14 00: EPWMxSOCB, read-only bit 13-12 00: SOCBPRD, don't care bit 11-10 00: EPWMxSOCA, read-only bit 9-8 01: SOCAPRD, 01 = generate SOCA on first event bit 7-4 0000: reserved bit 3-2 00: INTCNT, don't care bit 1-0 00: INTPRD, don't care */ EPwm5Regs.ETSEL.all = 0x0A00; // Enable SOCA to ADC /* bit 15 0: SOCBEN, 0 = disable SOCB bit 14-12 000: SOCBSEL, don't care bit 11 1: SOCAEN, 1 = enable SOCA bit 10-8 010: SOCASEL, 010 = SOCA on PRD event bit 7-4 0000: reserved bit 3 0: INTEN, 0 = disable interrupt bit 2-0 000: INTSEL, don't care */ ///////////////////////////////////////////////////////////////////////////////////////// EALLOW; PieVectTable.EPWM1_INT = &ePWMA_compare_isr; PieVectTable.ADCINT = &adc_isr; PieVectTable.TINT0 = &cpu_timer0_isr; EDIS; InitCpuTimers(); ConfigCpuTimer(&CpuTimer0,150,2000); PieCtrlRegs.PIEIER1.bit.INTx7 = 1; PieCtrlRegs.PIEIER1.bit.INTx6 = 1; PieCtrlRegs.PIEIER3.bit.INTx1 = 1; IER |= 5; EINT; ERTM; CpuTimer0Regs.TCR.bit.TSS = 0; // start timer0 while(1) { while(CpuTimer0.InterruptCount == 0); CpuTimer0.InterruptCount = 0; EALLOW; SysCtrlRegs.WDKEY = 0x55; // service WD #1 EDIS; } } void Gpio_select(void) { EALLOW; GpioCtrlRegs.GPAMUX1.all = 0; // GPIO15 ... GPIO0 = General Puropse I/O GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // ePWM1A active GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // ePWM1B active GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // ePWM2A active GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // ePWM2B active GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 1; // ePWM3A active GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 1; // ePWM3B active GpioCtrlRegs.GPAMUX2.all = 0; // GPIO31 ... GPIO16 = General Purpose I/O GpioCtrlRegs.GPBMUX1.all = 0; // GPIO47 ... GPIO32 = General Purpose I/O GpioCtrlRegs.GPBMUX2.all = 0; // GPIO63 ... GPIO48 = General Purpose I/O GpioCtrlRegs.GPCMUX1.all = 0; // GPIO79 ... GPIO64 = General Purpose I/O GpioCtrlRegs.GPCMUX2.all = 0; // GPIO87 ... GPIO80 = General Purpose I/O GpioCtrlRegs.GPADIR.all = 0; GpioCtrlRegs.GPBDIR.all = 0; // GPIO63-32 as inputs GpioCtrlRegs.GPCDIR.all = 0; // GPIO87-64 as inputs EDIS; } void Setup_ePWM(void){ EALLOW; SysCtrlRegs.WDKEY = 0xAA; // service WD #2 EDIS; EPwm1Regs.TBCTL.all = 0; EPwm1Regs.TBCTL.bit.CTRMODE = 0; // Count up and down operation (10) = 2 EPwm1Regs.AQCTLA.all = 0x0060; //set ePWM1A to 1 on “CMPA - up match” //clear ePWM1A on event “CMPA - down match” EPwm1Regs.AQCTLB.all = 0x0090; //clear ePWM1B on “CMPA - up match” //set ePWM1B to 1 on event “CMPA - down match” // we made reverse action to obtain complementary wave EPwm1Regs.DBRED = RisingEdgeDelay; // Rising Edge Delay = TTBCLK x DBRED EPwm1Regs.DBFED = FallingEdgeDelay; // Falling Edge Delay = TTBCLK x DBFED // TTBCLK = 13.3333ns to give 666ns delay we can use that number EPwm1Regs.DBCTL.all = 0x000B; // S5 = S4 = S2 = 0 S0 = S1 = S3 = 1 RED & FED active also Active high complementary mode also PWMxA is source for RED and FED EPwm2Regs.TBCTL.all = 0; EPwm2Regs.TBCTL.bit.CTRMODE = 0; // Count up and down operation (10) = 2 EPwm2Regs.AQCTLA.all = 0x0060; //set ePWM1A to 1 on “CMPA - up match” //clear ePWM1A on event “CMPA - down match” EPwm2Regs.AQCTLB.all = 0x0090; //clear ePWM1B on “CMPA - up match” //set ePWM1B to 1 on event “CMPA - down match” // we made reverse action to obtain complementary wave EPwm2Regs.DBRED = RisingEdgeDelay; // Rising Edge Delay = TTBCLK x DBRED EPwm2Regs.DBFED = FallingEdgeDelay; // Falling Edge Delay = TTBCLK x DBFED // TTBCLK = 13.3333ns to give 666ns delay we can use that number EPwm3Regs.TBCTL.all = 0; EPwm3Regs.TBCTL.bit.CTRMODE = 0; // Count up and down operation (10) = 2 EPwm3Regs.AQCTLA.all = 0x0060; //set ePWM1A to 1 on “CMPA - up match” //clear ePWM1A on event “CMPA - down match” EPwm3Regs.AQCTLB.all = 0x0090; //clear ePWM1B on “CMPA - up match” //set ePWM1B to 1 on event “CMPA - down match” // we made reverse action to obtain complementary wave EPwm3Regs.DBRED = RisingEdgeDelay; // Rising Edge Delay = TTBCLK x DBRED EPwm3Regs.DBFED = FallingEdgeDelay; // Falling Edge Delay = TTBCLK x DBFED // TTBCLK = 13.3333ns to give 666ns delay we can use that number EPwm1Regs.TBCTL.bit.CLKDIV = 0; EPwm2Regs.TBCTL.bit.CLKDIV = 0; EPwm3Regs.TBCTL.bit.CLKDIV = 0; CLKDIV = 1; EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0; EPwm2Regs.TBCTL.bit.HSPCLKDIV = 0; EPwm3Regs.TBCTL.bit.HSPCLKDIV = 0; HSPCLKDIV = 1; EPwm1Regs.TBPRD = (0.5 * deviceClockFrequency) / (switchingFrequency * CLKDIV * HSPCLKDIV); //the maximum number for TBPRD is (216 -1) or 65535 EPwm2Regs.TBPRD = (0.5 * deviceClockFrequency) / (switchingFrequency * CLKDIV * HSPCLKDIV); EPwm3Regs.TBPRD = (0.5 * deviceClockFrequency) / (switchingFrequency * CLKDIV * HSPCLKDIV); EPwm1Regs.CMPA.half.CMPA = EPwm1Regs.TBPRD / 2; // 50% duty cycle first EPwm2Regs.CMPA.half.CMPA = EPwm2Regs.TBPRD / 2; // 50% duty cycle first EPwm3Regs.CMPA.half.CMPA = EPwm3Regs.TBPRD / 2; // 50% duty cycle first EPwm1Regs.ETSEL.all = 0; EPwm1Regs.ETSEL.bit.INTEN = 1; // interrupt enable for ePWM1 EPwm1Regs.ETSEL.bit.INTSEL = 4; // interrupt on CMPA up match EPwm1Regs.ETPS.bit.INTPRD = 1; // interrupt on first event } interrupt void ePWMA_compare_isr(void) { EALLOW; SysCtrlRegs.WDKEY = 0xAA; // service WD #2 EDIS; ///////////////////////// EPwm1Regs.TBCTL.all = 0; EPwm1Regs.TBCTL.bit.CTRMODE = 2; // Count up and down operation (10) = 2 EPwm1Regs.AQCTLA.all = 0x0060; //set ePWM1A to 1 on “CMPA - up match” //clear ePWM1A on event “CMPA - down match” EPwm2Regs.TBCTL.all = 0; EPwm2Regs.TBCTL.bit.CTRMODE = 2; // Count up and down operation (10) = 2 EPwm2Regs.AQCTLA.all = 0x0060; //set ePWM1A to 1 on “CMPA - up match” //clear ePWM1A on event “CMPA - down match” EPwm3Regs.TBCTL.all = 0; EPwm3Regs.TBCTL.bit.CTRMODE = 2; // Count up and down operation (10) = 2 EPwm3Regs.AQCTLA.all = 0x0060; //set ePWM1A to 1 on “CMPA - up match” //clear ePWM1A on event “CMPA - down match” EPwm1Regs.TBCTL.bit.CLKDIV = 0; EPwm2Regs.TBCTL.bit.CLKDIV = 0; EPwm3Regs.TBCTL.bit.CLKDIV = 0; CLKDIV = 1; EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0; EPwm2Regs.TBCTL.bit.HSPCLKDIV = 0; EPwm3Regs.TBCTL.bit.HSPCLKDIV = 0; HSPCLKDIV = 1; EPwm1Regs.TBPRD = (0.5 * deviceClockFrequency) / (switchingFrequency * CLKDIV * HSPCLKDIV) ; //the maximum number for TBPRD is (216 -1) or 65535 EPwm2Regs.TBPRD = (0.5 * deviceClockFrequency) / (switchingFrequency * CLKDIV * HSPCLKDIV) ; EPwm3Regs.TBPRD = (0.5 * deviceClockFrequency) / (switchingFrequency * CLKDIV * HSPCLKDIV) ; ////////////////////////////////////////////////// sinus = (sin(2 * PI * (frequencyModulationRatio) * counter + phaseAngle) + 1) / 2; EPwm1Regs.CMPA.half.CMPA = EPwm1Regs.TBPRD - (magnitudeModulationRatio) * EPwm1Regs.TBPRD * sinus - 1;// sinus2 = (sin(2 * PI * (frequencyModulationRatio) * counter + 2 * PI / 3 + phaseAngle) + 1) / 2; EPwm2Regs.CMPA.half.CMPA = EPwm2Regs.TBPRD - (magnitudeModulationRatio) * EPwm2Regs.TBPRD * sinus2 - 1; // sinus3 = (sin(2 * PI * (frequencyModulationRatio) * counter + 4 * PI / 3 + phaseAngle) + 1) / 2; EPwm3Regs.CMPA.half.CMPA = EPwm3Regs.TBPRD - (magnitudeModulationRatio) * EPwm3Regs.TBPRD * sinus3 - 1; counter +=1; if( counter > ((1 / frequencyModulationRatio)-1)) counter = 0; EPwm1Regs.ETCLR.bit.INT = 1; PieCtrlRegs.PIEACK.all = 4; } interrupt void adc_isr(void){ EALLOW; SysCtrlRegs.WDKEY = 0xAA; // service WD #2 EDIS; voltage_vr1 = AdcMirror.ADCRESULT0; fundamentalSinusoidalMagnitude = voltage_vr1 * 3.3/4095; voltage_vr2 = AdcMirror.ADCRESULT1; fundamentalSinusoidalFrequency = voltage_vr2 * 55 / 4095 + 5; voltage_vr3 = AdcMirror.ADCRESULT2; phaseAngle = voltage_vr3 * 2 * PI / 4095; voltage_vr4 = AdcMirror.ADCRESULT3; switchingFrequency = ((voltage_vr4 * 97000) / 4095) + 4000; frequencyModulationRatio = fundamentalSinusoidalFrequency / switchingFrequency; magnitudeModulationRatio = fundamentalSinusoidalMagnitude / maximumDeviceVoltage; AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1; AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1; PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; } interrupt void cpu_timer0_isr(void) // ISR runs every 2000 ns (PWM-frequency = 500 KHz) // and is triggered by ePWM1 compare event // run - time of ISR is 630 ns { CpuTimer0.InterruptCount++; // Service watchdog every interrupt EALLOW; SysCtrlRegs.WDKEY = 0xAA; // Service watchdog #2 EDIS; // Acknowledge this interrupt to receive more interrupts from group 3 PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; } //=========================================================================== // End of SourceCode. //===========================================================================