Part Number: TMS320F280041
Hi, in the datasheet SPRS945C section 6.6 page 192 line 1.
The CPU is a 32-bit fixed-point processor which draws from the best features of digital signal processing.
Isn't F28004x CPU floating point?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280041
Hi, in the datasheet SPRS945C section 6.6 page 192 line 1.
The CPU is a 32-bit fixed-point processor which draws from the best features of digital signal processing.
Isn't F28004x CPU floating point?
Hi Howard,
The C28x CPU is fixed-point. Many C2000 devices (including F28004x) also contain an FPU which provides floating-point capability and is described in section 6.6.2 on the same page. It's perhaps non-intuitive to think of the CPU as fixed-point with a floating-point extension, but that's what it is. The datasheet is correct.
Regards,
Richard