This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F280049C: VDD Pins Circuit

Part Number: TMS320F280049C

Tool/software: Code Composer Studio

Hi e2e community,

when I tie VREGENZ to low I enable the internal LDO and the 1.2V are on the VDD pins. When I divide the VDD caps (minimum 12µF) through the number of VDD pins I'll get a minimum of 3µF cap per pin. Is it necessary to connect all VDD pins? Or is it enough to put a min. 3µF on each pin and don't connect all VDD pins together.

Best regards,

Tobias