This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: Serial communication not happening unless debugger is connected

Part Number: TMS320F28335

Hello,

                  I have programmed this controller to receive commands through UART(RS232) and upon reception, it is supposed to drive a gimbal. I have flashed the code in the controller and it was running fine but since last two days, the uart is not receiving the commands unless I connect the JTAG and i am not sure why it is behaving like that. Once the jtag is connected to the target, everything works fine, I even don't have to dump the code again. Any help would be greatly appreciated. 

Thanks,

Akhil