Part Number: TMS320F28035
Hi
1. Is the RAMP Generator PWMSYNC1/2/3/4 signal meaning PWM1SYNC?
2. Can PWM5/6 PWMSYNC signal synchronize with RAMPgenerator or not?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28035
Hi
1. Is the RAMP Generator PWMSYNC1/2/3/4 signal meaning PWM1SYNC?
2. Can PWM5/6 PWMSYNC signal synchronize with RAMPgenerator or not?
Thanks.
Daniel Fang said:1. Is the RAMP Generator PWMSYNC1/2/3/4 signal meaning PWM1SYNC?
The PWMSYNC signal used by the Ramp Generator is coming from the HRPWM portion of logic. It is not the same as the EPWMSYNCI/O signal.
Daniel Fang said:2. Can PWM5/6 PWMSYNC signal synchronize with RAMPgenerator or not?
Yes, all of the PWMSYNC signals on the device are available for use with the Ramp Generator.
1. Is the RAMP Generator PWMSYNC1/2/3/4 signal meaning PWM1SYNC?
[tlee]: The PWMSYNC signal used by the Ramp Generator is coming from the HRPWM portion of logic. It is not the same as the EPWMSYNCI/O signal.
[Daniel]: Is there document describe about this? I can't find this signal source on PWM&AD document.
2. Can PWM5/6 PWMSYNC signal synchronize with RAMPgenerator or not?
[tlee]: Yes, all of the PWMSYNC signals on the device are available for use with the Ramp Generator.
[Daniel]: Double check with you. It only has PWMSYNC1/2/3/4 on document. PWM5/PWM6 are not synchronize with Ramp Genarator? Am I right?
Daniel Fang said:1. Is the RAMP Generator PWMSYNC1/2/3/4 signal meaning PWM1SYNC?[tlee]: The PWMSYNC signal used by the Ramp Generator is coming from the HRPWM portion of logic. It is not the same as the EPWMSYNCI/O signal.
[Daniel]: Is there document describe about this? I can't find this signal source on PWM&AD document.
Since the PWMSYNC signal is generated in the HRPWM portion, the information is in the HRPWM Reference Guide. Look for HRPCTL[PWMSYNCSEL].
Daniel Fang said:2. Can PWM5/6 PWMSYNC signal synchronize with RAMPgenerator or not?[tlee]: Yes, all of the PWMSYNC signals on the device are available for use with the Ramp Generator.
[Daniel]: Double check with you. It only has PWMSYNC1/2/3/4 on document. PWM5/PWM6 are not synchronize with Ramp Genarator? Am I right?
No, all of the PWMs on the device (including PWM5 and PWM6) can generate PWMSYNC signals. They can all be used with the Ramp Generator. The figure was originally created for F2802x which only has 4 PWMs.
Daniel,
Just continue the PWMSYNCn enumeration for RAMPSOURCE. You can refer to the F28069 TRM register definition if you do not understand. They are implemented the same way.
-Tommy