Other Parts Discussed in Thread: TMS320F28379D
Tool/software: Code Composer Studio
I read in the documentation that if the card is connected to the USB cable it will blow the card. I have not yet connected the card but would like to know if this is still true. I have just receive the board and the serial number is sp8_1803622B. If I understand the documentation correctly this is version 1.3 and does no longer have this problem.
Therefore is it safe to connect it to the PCB USB and get powered from the PC USB +5V