This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-F28379D: Transmitting SPI Data from one Launchpad to another

Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE

Tool/software: Code Composer Studio

Hello,

I'm trying to use the example code "spi_loopback_cpu1" in ControlSuite to transmit a simple integer via SPI pins. The only modification I made to this code is to transmit the number 20 instead of zero. I initialized GPIO pins 16-19 for MOSI, MISO, CLK and STE, respectively on both of my launchpads and jumped wires between the pins (16 and 16 on launchpads 1&2 connected, etc). I then used Simulink's SPI receive function to retrieve the integer, but when running in external mode it is displaying zero because it is not receiving the data. Have I set up my hardware / software correctly to do this? Is there a way for me to check if an integer is being transmitted from the first launchpad to the MOSI pin?

Thanks,

Tyler