This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F280049: Device support for Blackhawk USB2000 Controller

Part Number: TMS320F280049

Tool/software: Code Composer Studio

Hi,

I would like to evaluate F280049 with a combination of CCSv8.2 and Blackhawk USB2000 Controller.
However, if you specify Blackhawk USB2000 Controller with Target Configuration setting
Only F280041, F280041C, F280045 can be selected.

Do I have to use emulators such as XDS110 (or XDS100v2), XDS200, etc. on devices with CLA?

Best Regards,
Koichi