Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: CONTROLSUITE, SFRA, DESIGNDRIVE, BOOSTXL-3PHGANINV
Hello,
My customer has some issues in his evaluation of a C2000 motor control solution:
The Launchpad with the 3PHGANINV board works fine with the motors, using code from ControlSuite.
Then they tried to use 2 legs only of the 3PHGANINV so to have an H-bridge. They programmed the epwm2 and epwm3 using Simulink and saw on an oscilloscope that the signals were correctly generated. But there is no power transferred, so the GAN FETs are not switching. Vin = 30 V was used. Could you help there?
Also, they would like to add their architecture to DesignDrive so to benefit from the SFRA features. Could you please advise how to proceed so they could use the SFRA and tune the compensator for their application?
Thank you,
François.