My first doubt is while using XBAR, why we use LOCK register for input and output. Why exactly we need LOCK BIT.
Secondly, I have two MCU of the same type on different PCB. The XBAR of MCU1 have one output (EXTSYNCOUT configured) and the other one is configured as input XBAR (EXTSYNCIN1).
My question is the pins of both MCU card connect directly or do we need any signal conversion like OPTO coupler etc. Please suggest me something by which I can send the signal and receive the signal securely.
The above I asked because while running in dry-run mode (No high power switching of IGBT) I saw all PWM are in the given phase shift But When I started with power switching mode of converters, it works very bad.
Currently, I connected the pins directly.
Also regarding code if possible please anyone provide me the exact configuration code in both MCU would be helpful for me.
Ashutosh Bhatt